SAFE.INVALIDATEPARAMS
Description
Invalidate the safety parameters. This command is executed when the SMM is in “operational” (SAFE.STATE is 6). It will invalidate the safety parameters and in consequence the SMM will go in a safe-state “configuration needed” (SAFE.STATE is 3).
Usage
Format is: SAFE.INVALIDATEPARAMS <user_name> <password> <date_and_time>
<user_name>: Username used to perform the safety parameters operation. Max 8 characters.
<password>: Password used for safety parameters operation. Min 8 characters, max 25 characters.
<date_and_time>: Format is YYYY-MM-DDThh:mm:ssZ.
Example: 2019-02-05T16:10:10Z which is 5th of February 2019, 16:10:10 UTC. Time zone must always be UTC.
Example: SAFE.INVALIDATEPARAMS john my_password 2019-02-05T16:10:10Z
Context
For more information refer to Validation and Downloading Safety Parameter Packages.
Related safety parameters:
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
No |