SAFE.VALIDATEPARAM
Description
Validates the safety parameters. Safety parameters must first be downloaded to the device.
Format is: SAFE.VALIDATE <user_name> <password> <date_and_time> <safe_id>
All parameters are mandatory. The drive will return an error if:
- Not enough parameters are provided
- Too many parameters are provided
- At least one of the parameter is out of range.
Note that the user_name and the password strings cannot contain any spaces.
- <user_name>: String of 8 bytes max
- <password>: String of 8 bytes min and 25 bytes max
- <date_and_time>: In the format defined by the RFC3339. The date must be in the UTC time zone.
Code
--> SAFE.VALIDATE john john_password 2019-02-22T10:58:30Z 16
Context
For more information refer to Validation and Downloading Safety Parameter Packages.
Related safety parameters:
- SAFE.CFGERROR
- SAFE.CHANGEPASSWORD
- SAFE.CLEARSAFEID
- SAFE.CRC
- SAFE.DEVICECRC
- SAFE.ERROR
- SAFE.INVALIDATEPARAMS
- SAFE.MONITOR#.AXIS
- SAFE.MONITOR#.DATA
- SAFE.MONITOR#.INSTANCE
- SAFE.MONITOR#.SOURCE
- SAFE.STATE
- SAFE.SWITCH
- SAFE.VALIDATIONLOG
- SAFE.VERIFYFW
- SAFEPARAM.IOFAILUREACKSOURCE
- SAFEPARAM.SAFEFIELDBUS.ACTIVATION
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
No |
Industrial Ethernet Information
All the validation fields must be filled in the following object. Note password entry must be written at the end. This will trigger the validation of the safety parameters.
|
Command |
Safety parameters validation - |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|---|
|
SAFE.VALIDATEPARAM |
username |
37c0h |
01h |
String(8) |
- |
- |
Read/Write |
No |
|
SAFE.VALIDATEPARAM |
date and time |
37c0h |
02h |
String(20) |
- |
- |
Read/Write |
No |
|
SAFE.VALIDATEPARAM |
SafeID |
37c0h |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
SAFE.VALIDATEPARAM |
password |
37c0h |
04h |
String(25) |
- |
- |
Read/Write |
No |