SAFE.ERROR

Description

Indicates the current error code of the SMM. Possible values of SAFE.ERROR are:

ID

Failure

Comments

0

No fault

 

1

Safe input fault

 

2

SDB failure

 

3

Safe output fault

 

4

STO output fault

 

5

Encoder startup timeout

The communication with the encoder reported a fatal problem. The timeout for the startup of the encoder occurred.

6

Encoder fault: No position available

No encoder position is available but is needed. No valid data is available.

7

Power supply fault (Vcc)

Undervoltage lead to a reset of the SMM.

8

Black-channel fault

The safe fieldbus detected a failure.

9..11

Fatal faults

No transmission to drive due to a lack of active communication.

12

Safety parameter invalid

The drive enters a safe state engaging the brake and removing power simultaneously. This happens when the configured sequence is unknown.

13

Brake output fault

 

14

Temperature fault

The temperature cools down when the drive is switched off.

15

Internal discrepancy

A discrepancy between two micro controllers on the SMM was detected.

16

FPGA not suitable

The FPGA software is not suitable for use with this SMM.

17

Internal fault

Error occurred.

18

I/O Fault

Error occurred which can be fixed.

19

Reserved

 

20

External memory fault

A failure occurred at the external non-volatile memory.

21

Manufacturing parameter invalid

The manufacturing data is invalid.

22

External discrepancy

The two inputs used for a dual input are different.

23

Brake current fault

The brake current is out of range.

24

Encoder fault: No speed available

No speed is available but needed. No valid data is available.

25

Encoder fault:
Invalid association

The association of the encoder to an axis is invalid. No valid data is available.

26

Encoder fault:
Invalid type

The encoder type is invalid. No valid data is available.

27

Deprecated

Note: Error only valid for SMM R_03-00-004.

27

Encoder fault:
Communication Channel 1

The encoder communication failed on channel 1. No valid data is available.

28

Deprecated

Note: Error only valid for SMM R_03-00-004.

28

Encoder fault:
Communication Channel 2

The encoder communication failed on channel 2. No valid data is available.

29

Encoder fault:
Communication timeout

The encoder reported a timeout in the communication. No valid data is available.

30

Encoder fault: H-DSL
Diagnostic test

Note: Error only valid for SMM R_03-00-004.

The H-DSL encoder reported an error in the diagnostic test. No valid data is available.

30

Encoder fault:
Diagnostic test

The encoder reported an error in the diagnostic test. No valid data is available.

31

Deprecated

Note: Error only valid for SMM R_03-00-004.

31

Encoder fault:
Event Channel 1

The encoder reported an error on channel 1. No valid data is available.

32

Deprecated

Note: Error only valid for SMM R_03-00-004.

32

Encoder fault:
Event Channel 2

The encoder reported an error on channel 2. No valid data is available.

33

Encoder fault:
Position Drift

The position between channel 1 and 2 is different. No valid data is available.

34

Encoder fault:
Startup error

The encoder reported a failed startup test. No valid data is available.

35

Encoder fault:
H-DSL encoder counter drift

Note: Error only valid for SMM R_03-00-004.

The message counters of the channels of an encoder differ more than expected.

35

Encoder fault:
Encoder counter drift

Note: Error only valid for SMM R_02-07-000.

The message counters of the channels of an encoder differ more than expected.

36

Encoder fault:
Encoder update rate

The encoder position update rate is out of tolerance.

The following errors are only valid for SMM R_03-00-004

37

Encoder fault: Position user unit overflow

The configured position user unit has overflowed the underlying integer type.

38

Encoder fault: Encoder CRC error

The encoder position or diagnostic data CRC is invalid.

39

Encoder fault: Invalid acceleration

The encoder acceleration is out of tolerance.

40

Encoder fault: Invalid EnDat recovery counter

The EnDat encoder recovery counter is out of tolerance.

41

Encoder fault: Invalid EnDat operation mode

The EnDat encoder mode is invalid.

42

Encoder fault: EnDat bad sequence

The EnDat communication sequence is invalid.

43

Encoder fault: Invalid EnDat clock period 

The EnDat encoder clock period is invalid.

44

Encoder fault: EnDat power supply error

The EnDat encoder power supply diagnostic has failed.

45

Encoder fault: EnDat F1 error bit

The EnDat encoder F1 error bit is set.

46

Encoder fault: EnDat F2 error bit

The EnDat encoder F2 error bit is set.

47

Encoder fault: EnDat dynamic sampling error

The EnDat encoder dynamic sampling has failed.

48

Encoder fault: Invalid H-DSL VPOS error

The H-DSL encoder has indicated an invalid safe position (vpos).

49

Encoder fault: H-DSL CRC error

The H-DSL encoder has indicated a CRC error on the safe channel (SCE).

50

Encoder fault: H-DSL STATUS 2 error

The H-DSL encoder has indicated an invalid safe position (STATUS2).

51

Encoder fault: H-DSL stuck-at fault

The H-DSL encoder has indicated a stuck-at fault.

52

Encoder fault: H-DSL SUM fault

The H-DSL encoder has indicated an invalid safe position (SUM).

53

Encoder fault: H-DSL STx error

The H-DSL encoder has indicated an invalid safe position (STx).

54

Encoder fault: H-DSL register operation error

An H-DSL encoder register operation has failed.

55

Encoder fault: H-DSL startup diagnostic error

The H-DSL encoder has failed to perform the startup test.

56

Encoder fault: H-DSL unexpected error

The H-DSL encoder has indicated an unexpected reset.

57

Encoder fault: Speed user unit overflow

The configured speed user unit has overflowed the underlying integer type.

58

Encoder fault: Acceleration user unit overflow

The configured acceleration user unit has overflowed the underlying integer type.

Code

--> SAFE.ERROR
0

Context

For information on validation refer to Safety Faults, Safety Warnings.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

SAFE.ERROR

37c4h

00h

Unsigned16

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3803

1

3803 (0xedb)

SAFE.ERROR

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

SAFE.ERROR

3803

Unsigned16

Read Only

-