SAFE.SWITCH

Description

Returns a value defined by the state of the two rotary switches S1 and S2. The returned value is equal to (10*S1 + S2). When this value is validated, it becomes the SafeID.

Code

--> SAFE.SWITCH
16

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

0 or 1

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable

EtherCAT COE and CANopen

SAFE.SWITCH

0x37C2

0x0

USINT

-

-

RO

-