SAFE.DEVICECRC
Description
Returns the Cyclic Redundancy Check (CRC) of the device’s safety parameters dedicated to this device stored inside the complete safety parameters file. If there are no safety parameters available, the CRC returned is 0.
Code
--> SAFE.DEVICECRC 0x72d5a4df
Context
For information on CRC and validation refer to Validation.
Related safety parameters:
- SAFE.CFGERROR
- SAFE.CHANGEPASSWORD
- SAFE.CLEARSAFEID
- SAFE.CRC
- SAFE.ERROR
- SAFE.INVALIDATEPARAMS
- SAFE.MONITOR#.AXIS
- SAFE.MONITOR#.DATA
- SAFE.MONITOR#.INSTANCE
- SAFE.MONITOR#.SOURCE
- SAFE.STATE
- SAFE.SWITCH
- SAFE.VALIDATEPARAM
- SAFE.VALIDATIONLOG
- SAFE.VERIFYFW
- SAFEPARAM.IOFAILUREACKSOURCE
- SAFEPARAM.SAFEFIELDBUS.ACTIVATION
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
All |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |