SAFE.VERIFYFW
Description
Sets the username, password, and checksum that is used for an SMM firmware update. WorkBench automatically sends this command when using the firmware update dialog window. Once this command is sent, SMM firmware must be sent by HTTP within 30 seconds.
Context
Related safety parameters:
- SAFE.CFGERROR
- SAFE.CHANGEPASSWORD
- SAFE.CLEARSAFEID
- SAFE.CRC
- SAFE.DEVICECRC
- SAFE.ERROR
- SAFE.INVALIDATEPARAMS
- SAFE.MONITOR#.AXIS
- SAFE.MONITOR#.DATA
- SAFE.MONITOR#.INSTANCE
- SAFE.MONITOR#.SOURCE
- SAFE.STATE
- SAFE.SWITCH
- SAFE.VALIDATEPARAM
- SAFE.VALIDATIONLOG
- SAFEPARAM.IOFAILUREACKSOURCE
- SAFEPARAM.SAFEFIELDBUS.ACTIVATION
Usage
Format is: SAFE.VERIFYFW <user_name> <password> <checksum> <user_name>: Username used to perform the safety firmware update. Max 8 characters. <password>: Password used for safety firmware update. Min 8 characters, max 25 characters. <checksum>: Checksum of the firmware update binary.
Example: SAFE.VERIFYFW john my_password 0xa1878800
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
|
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non-Volatile Memory |
No |