SAFE.CFGERROR
Description
In case the safety parameters validation fails due to invalid configuration, this parameter returns information about which parameters failed to validate and why.
Code
--> SAFE.CFGERROR
Parameter: [PARAMETER_NUMBER] PARAMETER_KEYWORD_NAME
Axis: AXIS_ID
Instance: INSTANCE_ID
Error: [ERROR_NUMBER] ERROR_DESCRIPTION
Context
For information on validation refer to Validation.
Related safety parameters:
- SAFE.CHANGEPASSWORD
- SAFE.CLEARSAFEID
- SAFE.CRC
- SAFE.DEVICECRC
- SAFE.ERROR
- SAFE.INVALIDATEPARAMS
- SAFE.MONITOR#.AXIS
- SAFE.MONITOR#.DATA
- SAFE.MONITOR#.INSTANCE
- SAFE.MONITOR#.SOURCE
- SAFE.STATE
- SAFE.SWITCH
- SAFE.VALIDATEPARAM
- SAFE.VALIDATIONLOG
- SAFE.VERIFYFW
- SAFEPARAM.IOFAILUREACKSOURCE
- SAFEPARAM.SAFEFIELDBUS.ACTIVATION
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-00-00-000 |
Implemented in SMM revision v0.32 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Stored in Non-Volatile Memory |
No |