CIP_Axis_Enable AOI
Description
The CIP_Axis_Enable instruction requests to enable the AKD2G-SPI axis via the CIP_Axis_State_Machine AOI.
Compatibility
The CIP_Axis_Enable AOI is only compatible with AKD2G-SPI drives when used with Motion Supported PLCs with Studio 5000 and the CIP Sync connection.
Required Command Source and Operation Mode
AXIS#.CMDSOURCE = Fieldbus
AXIS#.OPMODE = Position
The CIP_Axis_Enable AOI passes a RequestedAction of 2 to the corresponding CIP_Axis_State_Machine AOI for the given axis. When the axis status bit Operation Enabled and Quick Stop status bits are True then the CIP_Axis_Enable command is successful and the .DN bit is set. If the axis status bit Operation Enabled does not transition to True in a timely manner, then a command timeout for the CIP_Axis_Enable AOI is declared and its .ER bit is set.
The CIP_Axis_Enable instruction execution time may require multiple scans (additional 300-350 ms) due to the required fieldbus communication time and time for the drive’s axis output and servo loop to be activated.
Operands
These entries are required by the user.
|
Operand |
Data Type |
Format |
Description |
|---|---|---|---|
|
CIP_Axis_Enable |
CIP_Axis_Enable |
Tag |
Tag name for instance of the AOI. |
|
Axis |
CIP_Axis |
Tag |
User tag defined in the Axis1 or Axis2 field of the CIP_Drive_Comms AOI. |
|
Error_Description |
STRING |
Tag |
User tag to display the string error code description. In run-time when the mouse cursor is hovered over the tag the string can be monitored.
|
Structure
The following fields are not entered by the user and are populated automatically with Read Only data once the Operands (in the Operand table for this AOI) are entered or presented as output data (bits).
|
Mnemonic |
Type |
Format |
Description |
|---|---|---|---|
|
.EnableIn |
Input |
BOOL |
The Enable Input bit indicates the instruction is enabled. |
|
.EnableOut |
Output |
BOOL |
The Enable Output bit is the output of the Enable Input (.EnableIn) bit. |
|
.DN |
Output |
BOOL |
Turns on when the enabled response is returned (enabled state acknowledged). Set when the status bits Axis.Status.Operation_Enabled and Axis.Status.Quick_Stop bits are both ON. |
|
.ER |
Output |
BOOL |
The .ER bit is set if the Operation Enabled status bit 2 in the Status Word is not confirmed ON in the time set by the Command Timeout preset. |
|
Error_Code |
Output |
SINT |
0 = No Error, 1 = Command Timeout, 2 = Axis Faulted |
Changes to Axis Status Bits and Control Word bits Description
-
All status bits are updated from the drive. See Status Word in CIP Sync Response Assembly Data Structure (106) for more information.
-
Control Word bits descriptions and functions are described under Control Word in CIP Sync Command Assembly Data Structure (105).
On Enable the axis enters the Operation Enabled state and the status bits are as follows:
| Bit | Name | Status |
|---|---|---|
| 0 | Ready To Switch On | ON |
| 1 | Switched On | ON |
| 2 | Operation Enabled | ON |
| 5 | Quick Stop | ON |
| 6 | Switch On Disabled | OFF |
See the sections "States of the state machine" and "Mode-dependent bites in the statusword" in CIP Sync: State Machine for more information.
Example of Usage/Programming Guidelines
In the Sample project the CIP_Axis_Enable AOI is used in the subroutine for the given axis under MainTask → MainProgram → Axis1_Routine or Axis2_Routine.
Subroutines are called in the MainRoutine_with_CIP_State_Machines routine under MainTask → Main Program.
As demonstrated below, the best practice for the CIP_Axis_Enable AOI is to use a conditional N.O. Contact as a trigger (Ax1_Enable_Toggle in the example below) and then use a One Shot (ONS) to trigger the CIP_Axis_Enable AOI .EnableIn. A parallel branch is implemented around the N.O. Contact and One Shot to seal-in the .EnableIn of the AOI until execution completes (.DN; Done) or fails (.ER; Error). An interlock is shown using the AXIS_ONE.Status.Fault status bit as a N.C. Contact so the CIP_Axis_Enable cannot be triggered if the axis is faulted.
An additional rung provides a way to monitor the enable state in the ladder based on the AXIS_ONE.Status.Operation_Enabled status bit in the axis status word and when it is True (ON) a coil in the ladder named Axis1_Enabled turns ON. Note, AXIS_ONE is the name given to Axis1 in the CIP_Drive_Comms as an alias in the Sample project for all other Kollmorgen CIP_Axis AOIs to use for that axis.
Figure 1: Example: Axis1_Routine with CIP_Axis_Enable AOI
Troubleshooting
The condition for the Error (.ER) bit to be set for the CIP_Axis_Enable AOI:
If the Axis.Status.Operation_Enabled bit does not turn ON in 2000 msec then declares a command timeout error.
Step Summary
|
Step Number |
Operation/Result |
|---|---|
|
0 |
Clear bits and error codes |
|
1 |
Set the Axis.RequestedAction to 2 (Enable) |
|
2 |
Monitor Axis.Status.Operation_Enabled and Axis.Status.Quick_Stop to determine success (DN) or command timeout (ER) |
|
-1 |
Error (Command Timeout or Axis Faulted) |
Revision History
| Revision Number | Description/Notes | Date of Revision |
|---|---|---|
| v1.5 | Initial release | 03-14-2024 |