CIP_Axis_State_Machine AOI

  • Each AKD2G Axis requires a corresponding CIP_Axis_State_Machine AOI to receive requested actions (commands) from the supplementary Kollmorgen CIP Axis AOIs.
  • This generates operations such as Enable, Disable, Home, Fault Reset, Quick Stop, Enable Streaming, and Disable Streaming.

screen capture of the CIP_Axis_State_Machine AOI

Use the CIP_Axis_State_Machine instruction to:

  • Synchronize the AKD2G axis’ AXIS#.EIP.STREAMPERIOD with the Motion Group’s CoarseUpdatePeriod.
  • Synchronize the AKD2G axis’ AXIS#.EIP.UNWIND where:
    • If the Virtual Axis is rotary, AXIS#.EIP.UNWIND = Position Unwind value of the Virtual Axis.
    • If the Virtual Axis is linear, the Position Unwind of the Virtual Axis is not used and the AXIS#.EIP.UNWIND is set to 2,000,000,000.
  • Monitor the axis’ State Machine including:
    • CIP_Axis_State_Machine AOI’s IP, DN, and ER bits
    • Axis status bits
    • AxisControlWord bits
    • RequestedAction
    • StateMachineErrorCode (if State Machine Error is present)
    • StateMachineErrorDescription (if State Machine Error is present)
    • StateMachineCurrentState and StateMachineCurrentStateDescription

Compatibility

The CIP_Axis_State_Machine AOI is only compatible with AKD2G-SPI drives when used with Motion Supported PLCs with Studio 5000 and the CIP Sync connection.

Required Command Source and Operation Mode

  • AXIS#.CMDSOURCE = Fieldbus
  • AXIS#.OPMODE = Position

The CIP_Axis_State_Machine AOI is always enabled in the Ladder routine under MainTask > MainProgram by the AOI’s EnableIn being tied to the left rail.

  • The Sample project includes a CIP_Axis_State_Machine AOI for each axis in a routine under the MainTask > MainProgram called MainRoutine_with_CIP_State_Machines.

The CIP_Axis_State_Machine provides this functionality:

  • Sets the Stream Period of the Axis in the AKD2G drive (on prescan) via internal MSG instructions inside the CIP_Axis_State_Machine AOI.
  • Receives a Request Action from the supplemental KollmorgenAOIs to move within the CIP Sync: State Machine from one state to another to generate certain operations (i.e., fault reset).
  • Monitors and displays the Status bits for the axis based on the current state.
  • Displays the:

Operands

These entries are required by the user.

Operand

Data Type

Format

Description

CIP_Axis_State_Machine

CIP_Axis_State_Machine

Tag

Tag name for this instance of the AOI.

Axis

CIP_Axis

Tag

User tag for AKD2G drive’s axis defined in the CIP_Drive_Comms AOI fields Axis1 or Axis2.

VirtualAxis

AXIS_VIRTUAL

Tag

  • User tag defining the name of the Virtual Axis declared in the MotionGroup.
  • This generates the motion trajectory of the corresponding AKD2G drive’s axis or if unused in the Ungrouped Axes.

MotionGroup

MOTION_GROUP

Tag

User tag defining the name of the MotionGroup controlling the given AKD2G drive.

UpdatePeriodMsg

MESSAGE

Tag

User tag defining the name of the UpdatePeriod MSG internal to the CIP_Axis_State_Machine AOI.

UnwindMsg

MESSAGE

Tag

User tag defining the name of the Unwind MSG internal to the CIP_Axis_State_Machine AOI.

StateMachineErrorDescription

STRING

Tag

StateMachineCurrentStateDescription

STRING

Tag

Structure

These fields are not entered by the user and are populated automatically with Read Only data once the Operands (in the Operand table for this AOI) are entered or presented as output data (bits).

Mnemonic

Type/Usage

Data Type

Description

.EnableIn

Input

BOOL

The Enable Input bit indicates the instruction is enabled.

.EnableOut

Output

BOOL

The Enable Output bit is the output of the Enable Input (.EnableIn) bit.

.IP

Output

BOOL

In Process bit.

.DN

Output

BOOL

Done bit.

.ER

Output

BOOL

Error bit.

RequestedAction

Output

INT

StateMachineErrorCode

Output

INT

StateMachineCurrentState

Output

INT

AxisControlWord

Output

INT

.AxisReadyToSwitchOn

Output

BOOL

.AxisSwitchedOn

Output

BOOL

.AxisOperationEnabled

Output

BOOL

.AxisFaulted

Output

BOOL

.AxisVoltageEnabled

Output

BOOL

.AxisQuickStop

Output

BOOL

.AxisSwitchedOnDisabled

Output

BOOL

.AxisWarning

Output

BOOL

.AxisSTO

Output

BOOL

.AxisRemote

Output

BOOL

.AxisTargetReached

Output

BOOL

.AxisInternalLimitActive

Output

BOOL

.AxisHomeAttained

Output

BOOL

.AxisHomingError

Output

BOOL

.AxisMotionModeHoming

Output

BOOL

.AxisMotionModeCyclicPosition

Output

BOOL

.AxisFollowingError

Output

BOOL

.AxisStreamingActive

Output

BOOL

State Machine Requested Actions

Requested Action #

Requested Action

Used By AOI

State Machine AOI Internal Mode

0

Idle

CIP_Axis_Disable_Streaming

Mode 0

1

Disable

CIP_Axis_Disable

Mode 1

2

Enable

CIP_Axis_Enable

Mode 2

3

Reset Faults

CIP_Axis_Fault_Reset

Mode 3

4

Quick Stop

CIP_Axis_Quick_Stop

Mode 4

5

Start Home Move

CIP_Axis_Home

Mode 5

6

Enable Cyclic Position Streaming

CIP_Axis_Enable_Streaming

Mode 6

In most cases after the Requested Action is completed, the reported RequestedAction is 0 (Idle).

Figure 1: State Machine RequestedAction shown in the field highlighted in the AOI.

State Machine Current States and Descriptions

Current State #

State Description

0

Not Ready To Switch On

1

Switch On Disabled

2

Ready To Switch On

3

Switched On

4

Operation Enabled

5

Quick Stop Active

6

Fault Reaction Active

7

Faulted

Hover the mouse cursor over the tag for StateMachineCurrentStateDescription to view the Current State Description.

Execution

Changes to Axis Status Bits and Control Word bits Description

Example of Usage/Programming Guidelines

From the Sample project under MainTask > MainProgram, a routine named MainRoutine_with_CIP_State_Machines contains the CIP_Axis_State_Machine AOIs for each axis (only Axis1 shown below).

There are JSR (Jump To Subroutines) where each subroutine is the ladder logic for each respective axis ( i.e., Axis1_Routine, Axis2_Routine, etc.)

The CIP_Axis_State_Machine AOI(s) are tied unconditionally to the left rail and execute on every scan.

The UpdatePeriodMSG and UnwindMsg messages inside the CIP_Axis_State_Machine AOI must be configured correctly to point to the correct:

  • Attribute IDs (of the parameters for the axis in the AKD2G drive).
  • Module path for the CIP_Axis_State_Machine to operate without error (.ER).

Troubleshooting

  • State Machine Error Codes are found in the StateMachineErrorCode and StateMachineErrorDescription fields.
  • Hover the mouse cursor over the StateMachineErrorDescription tag to view the error description.

Error Code Syntax: XYY

  • X = Mode the Fault occurs in

  • YY = Error ID

State Machine Error Codes and Error Descriptions

Error Code

Error Description

Additional Description

Mode

0

No Error

 

N/A

101

In Fault Reaction Active state while trying to disable.

 

1 - Disable Axis

102

In Fault state while trying to disable.

 

1 - Disable Axis

201

In Fault Reaction Active state while trying to enable.

 

2-Enable Axis

202

In Fault state while trying to enable.

 

2-Enable Axis

401

Not in Operation Enable or Quick Stop state after requesting Quick Stop State.

 

4-Quick Stop

501

Homing Error status bit is set.

Indicates the home routine failed.

5-Home

601

Not In Operation Enabled state.

Attempt to stream when axis is not enabled.

6-Cyclic Position

602

Home Attained status bit is cleared.

Attempt to enable streaming when not homed.

6-Cyclic Position

603

Cyclic Position Following Error bit is set.

Status bit 13 indicates a following error occurred.

6-Cyclic Position

604

Update Period MSG error.

  • UpdatePeriodMsg attempt to write the stream period failed and is in error.
  • Attempt to stream failed.

6-Cyclic Position

605

Unwind MSG error.

  • UnwindMsg attempt to write the position unwind value failed and is in error.
  • Attempt to stream failed.

6-Cyclic Position

701

Error in MRP instruction used to synch drive axis with virtual axis, (while) not streaming.

  • Error in the internal MRP (Motion Redefine Position) instruction that synchronizes the AKD2G drive axis with the virtual axis when not streaming.
  • The MRP is used to set the virtual axis command to the AKD2G drive axis’ position feedback when not streaming.
  • Most common cause of error is both:
    • The rotary axis’ modulo is not turned on.
    • The virtual axis command is synchronized to a drive axis position feedback outside the position unwind range.

N/A

Step Summary

  • None

Revision History

Revision Number

Description/Notes

Date of Revision

v1.5

Initial release

March 2024