System Requirements
KAS-IDE and KAS Simulator are compatible with any PC having this minimum hardware.
These are the minimum system requirements for the KAS-IDE.
|
Component |
Description |
|---|---|
|
Supported Operating Systems |
|
|
Connectivity |
|
|
Display |
|
|
Hard Disk |
Free space required on hard disk:
|
|
Network |
Internet connection for downloading and updating WebView2 Runtime. |
|
Processor |
Intel Pentium M or equivalent processor at 1.5GHz or greater. |
|
RAM |
|
|
Software |
|
|
Web Browser |
|
-
-
- Better results are achieved with OpenGL and 3D cards.
- A 100MB or 1GB network is required to allow the KAS-IDE to Runtime communication to work in all conditions.
The AKD WorkBench AutoTuner and Scope both require 100MB of bandwidth to function properly.
-
-
- See Connect Remotely about the ports used by the KAS.
- The ports may need to be opened to support connecting to a controller from an external network.
Digital Signatures
The KAS-IDE Installer and the executables are digitally signed to protect the integrity of these files and identify the distributor of the software components.
The digital signature appears as part of the file properties.
Figure 1: Example: KAS Setup Properties Digital Signature