Connect Remotely
You can connect to a controller from an external network using VPN or other tunneling protocol.
You must open these ports which are used by KAS to connect to a controller:
|
Port |
Component / Protocol Using the Port |
|---|---|
|
AKD PDMM and PCMM: 80 PCMM2G: 80, 443 |
KAS-IDE: |
|
502 |
HMI and other Modbus devices to communicate with Modbus TCP. |
|
2222 |
EtherNet/IP communication. |
|
4002 |
KAS-IDE: Oscilloscope variable monitoring. |
|
4003 |
KAS-IDE:
|
|
PCMM2G: 4840 (user-configurable) AKD PDMM and PCMM: N/A |
OPC UA Server Communications:
|
|
9900 |
KAS-IDE:
|
|
34962 |
PROFINET communication. |
|
34964 |
PROFINET communication. |
|
44848 |
EtherNet/IP communication. |