System Library

These tables list the System functions and function blocks:

See PrintMessage - Generates a log message with any wanted strings in the Log Messages tabs window.

Controller

Name

Description

ClearCtrlErrors

Clears the list of active errors and alarms on the controller.

CtrlReadBoolPar

Reads an Axis Boolean property of a Pipe Network Axis.

GetCtrlErrors

Get a list of the active errors and alarms on the controller.

GetCtrlInfo

Get the serial, model, and/or part number of the controller.

GetCtrlPerf

Returns controller CPU performance statistics.

File

Name

Description

FileClose

Closes an open file.

FileCopy

Copies a file's contents to a new file.

FileDelete

Removes a file from the file system.

FileEOF

Test if the end of the file is reached in a file that is open for reading.

FileExists

Tests if a file exists.

FileOpenA

Create or open a file in append mode.

FileOpenR

Open a file for reading.

FileOpenW

Create or reset a file and open it for writing.

FileReadBinData

Read binary data from a file.

FileReadLine

Reads a string value from a text file.

FileRename

Renames a file.

FileSeek

Sets the current position in an open file.

FileSize

Gets the size of a file.

FileWriteBinData

Write binary data to a file.

FileWriteLine

Writes a string value to a text file.

Profiling

Name

Description

Stopwatch

Measures the elapsed time between two events and gathers basic statistics when measurements are repeated.

Recipe Function Blocks

Name

Description

RecipeApplyInstance

Copy values to from a recipe instance to the program data.

RecipeClose

Close a recipe object.

RecipeOpen

Open a recipe file and create a recipe object.

RecipeQuickLoad

Load a recipe file and immediately apply the items it contains.

RecipeSave

Save a recipe object to a file.

RecipeSaveRetainVars

Save all retain variables, and their values, into a new recipe file.

RecipeStoreInstance

Store the present values of the program data in a recipe instance.

TCP/IP Sockets

Name

Description

TcpAccept

Performs the accept operation.

TcpBinReceive

Receives characters over a socket connection.

TcpBinSend

Sends characters over a socket.

TcpClose

Closes and releases a socket.

TcpConnect

Creates a new socket and performs the connect operation.

TcpIsConnected

Tests if a client socket is connected.

TcpIsValid

Tests if a socket is valid.

TcpListen

Creates a new socket by performing the bind and listen operations.

TcpReceive

Receives characters over a socket connection.

TcpSend

Sends characters over a socket.

UDP

Name

Description

udpAddrMake

Build an address buffer for UDP functions.

udpClose

Closes a socket.

udpCreate

Creates a UDP socket.

udpIsValid

Tests if a socket is valid.

udpRcvFrom

Receives a UDP telegram.

udpRcvFromArray

Receives a byte array through UDP.

udpRcvFromVar

Receives the contents of a variable from another controller through UDP.

udpSendTo

Sends a UDP telegram.

udpSendToArray

Sends a byte array through UDP.

udpSendToVar

Sends the contents of a local variable to another controller through UDP.