Unexpected complex data in expression.
or
Boolean expression expected after IF.
These errors indicate that the IF THEN ELSE ELSIF END_IF condition used in the application code does not evaluate to a BOOL expression.
Controller:------------- Compile PLC ---------------
…
Controller:PLC:MCFB_Jog
Controller:PLC:MCFB_Jog: (16): Unexpected complex data in expression
Controller:PLC:MCFB_Jog: (16): Boolean expression expected after IF
Controller:PLC:MCFB_Jog: (19): END_IF: New statement expected
Controller:PLC:Error(s) detected
Controller:------------- PLC failed ---------------
Controller:------------- Device compile failed ---------------
...
Project compile failed
This compile error can happen when a non-compliant syntax is used for verifying the function block outputs.
- In KAS v4.0 and earlier releases, it was possible to use the function block return statement in the same way as function return values.
- This could result in undefined behavior.
- In KAS v4.0 and later releases, the compiler generates a an Unexpected complex data in expression error for non-compliant syntax.
IEC 61131-3 Non-Compliant Syntax:
If inst_functionBlock(myVar1) Then
// ...
End_If;IEC 61131-3 Compliant Syntax:
inst_functionBlock(myVar1);
If inst_functionBlock.Q Then
// ...
End_If;
Error Correction
- Identify the code that caused compile error.
- If the error is due to non-compliant syntax, replace this code using compliant syntax for the corresponding function block.
Example: Non-compliant Syntax
IF Inst_r_trig(Inst_TON.Q) THEN
Inst_DriveParamRead( TRUE, any_to_int(Inst_MC_ReadParam.Value), 'DRV.FAULT1' );
END_IF;
Example: Compliant Syntax
Inst_r_trig(Inst_TON.Q);
IF Inst_r_trig.Q THEN
Inst_DriveParamRead( TRUE, any_to_int(Inst_MC_ReadParam.Value), 'DRV.FAULT1' );
END_IF;
-
-
If you prefer to not update a KAS project to use compliant syntax, select the Allow non-compliant syntax to evaluate function block outputs check box in the Project Settings dialog box.
-
-
UDFBs and libraries can have improper syntax.
These Kollmorgen UDFBs have been corrected and can be re-imported into the application code.
See Re-import Kollmorgen UDFBs.
See Also