AXIS#.IL.COMPTABLE.ENABLE

Description

AXIS#.IL.COMPTABLE.ENABLE returns the current output of the cogging compensation/torque compensation table.

See AXIS#.IL.COMPTABLE.DATA for more information how the table operates.

Example

Once a cogging map/torque map has been loaded, it can be turned on for Axis 1 by setting to 1:

-->AXIS1.IL.COMPTABLE.ENABLE 1

To disable a cogging map/torque map that has been loaded, set the same keyword to 0:

-->AXIS1.IL.COMPTABLE.ENABLE 0

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COMPTABLE.ENABLE

500ah

19h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5838

1

5838 (0x16ce)

AXIS1.IL.COMPTABLE.ENABLE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.COMPTABLE.ENABLE

5838

Unsigned8

Read/Write

-