MOTOR.TEMPFAULT
Description
This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensor.
A zero value prevents any fault from being issued.
-
-
For firmware versions 01-09-00-000 and later, this parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.
General Information
|
Type |
NV Parameter |
|
Units |
Ω |
|
Range |
0 to 2,000,000,000 Ω |
|
Default Value |
0 Ω = switched off |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | No |
| Index/Subindex | Object Start Version |
|---|---|
| 3586h/0 | M_01-00-00-000 |
Related Topics