MOVE.MOVING
Description
MOVE.MOVING only indicates whether or not the commanded motion profile for MOVE.GOREL, MOVE.GOABS, MOVE.GOHOME, and MOVE.GOVEL is complete. Even when the commanded motion profile is completed (MOVE.MOVING = 0), there may still be motor motion as the result of settling time and/or electronic gearing. MOVE.MOVING is not applicable for EGEAR commands.
0 - commanded motion complete
1 - move in progress
MOVE.MOVING is high when:
- The trajectory generator is active and the motor is moving, and for MOVE.DWELLTIME+ MOVE.SCURVETIME afterwards. The motor is considered not moving on exactly the same condition that stops the controlled stop (VL.FBFILTER is below CS.VTHRESH uninterrupted for at least CS.TO ).
- A controlled stop is being executed after hitting a limit switch. Execution stops when VL.FBFILTER is below CS.VTHRESH uninterrupted for at least CS.TO. The Controlled Stop parameters and settings are on the Enable/Disable screen in WorkBench.
-
-
MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.
Example
MOVE.RELATIVEDIST = 10000 MOVE.GOREL While MOVE.MOVING : Wend Pause(0.5) MOVE.RELATIVEDIST = -MOVE.RELATIVEDIST MOVE.GOREL
General Information
|
Type |
R/O |
|
Units |
N/A |
|
Range |
0 or 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1118 |
No | 32 bit | No |
M_01-05-11-000 |
Related Topics
MOVE.INPOSITION | MOVE.INPOSITION | MOVE.GOREL | MOVE.GOABS | MOVE.GOHOME | MOVE.GOVEL