AIN.DEADBANDMODE

Description

When AIN.DEADBANDMODE is set to 0, and the value of the analog input is less than the value of AIN.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the AIN.DEADBAND, then the analog command will be generated using the scaling specified.

When AIN.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the deadband value. When the input is greater than the deadband, the output is equal to (Input - Deadband) * Scaling. Below are illustrations of this behavior.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

AIN.DEADBAND

Start Version

M_01-03-06-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

5251h /0

M_01-03-06-000

Fieldbus

Address

Attributes Signed?

Profinet

2593

Word No
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 594 2 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

1186

No 16 bit No

Related Topics

Analoger Eingang

Blockschaltbild für den Positions-/Geschwindigkeitsregelkreis

AIN.DEADBAND