BODE.IFLIMIT

Description

When BODE.MODE is set to 5, the firmware monitors the drive current (IL.CMD ). When IL.CMD goes above BODE.IFTHRESH, an internal counter records the length of time IL.CMD was above BODE.IFTHRESH. If the internal counter reaches BODE.IFLIMIT, Fault 133 – Instability during Autotune will be generated.

The smaller the BODE.IFLIMIT, the quicker Fault 133 will be generated when IL.CMD exceeds BODE.IFTHRESH.

Example

Set BODE.IFTHRESH to 6 Amps:

-->BODE.IFTHRESH 6

Set BODE.IFLIMIT to 0.500 seconds:

-->BODE.IFLIMIT 0.5

Set BODE.MODE to 5 to enable stability detection:

BODE.MODE 5

General Information

Type

R/W Parameter

Units

s

Range

0.001 to 60.000

Default Value

0

Data Type

Decimal

Start Version

M_01-02-10-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2648

DWord Yes
sercos® III 4 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 649 4 Byte Signed Float

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1296

No 32 bit Yes

M_01-06-03-000

Related Topics

Verwendung des automatischen Tunings

Using the Performance Servo Tuner: Advanced

F133

BODE.MODE,BODE.MODETIMER, BODE.IFTHRESH, BODE.VFLIMIT, BODE.VFTHRESH