CAP0.EN, CAP1.EN

Description

This parameter enables or disables the related capture engine. After each successful capture event, this parameter is reset to 0 and must be activated again for the next capture. Also note that CAP0.PLFB, CAP1.PLFB is set to 0 when this parameter is set to 1.

0 = Disable

1 = Enable

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Boolean

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Paramter

Fieldbus

Address

Attributes Signed?
CAP0.EN Profinet

2028

Byte No
sercos® III 2 Octets
CAP1.EN Profinet 2041 Byte
sercos® III 2 Octets
Fieldbus Parameter Instance Data Size Data Type
EtherNet/IP CAP0.EN 29 1 Byte Integer
CAP1.EN 42

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus 56 CAP0.EN No 8 bit No

M_01-03-00-000

82 CAP1.EN

Related Topics

Verwendung der Positionserfassung