DIN1.PARAM TO DIN7.PARAM
Description
This parameter sets a value that is used as an extra parameter for digital inputs nodes.
-
-
AKD-N only supports DIN1 to DIN3.
Example
The digital input mode "Start motion task" is used to start a motion task. This mode uses an extra parameter as the ID of the motion task to be started.
Range
DINx.PARAM is used for various Digital Input modes. This causes the parameter’s range to change based on the current Digital Input mode selected with the corresponding DINx.MODE
Listed below are the possible ranges for each Digital input mode.
If an input mode is not listed, then the default range above is used.
| Input Mode | Min | Max | Notes |
|---|---|---|---|
| 2 | 0 | 128 | |
| 6 | Velocity Min | Velocity Max | This value changes based on user selected velocity units. |
| 9 | 0 | 4 | |
| 17 | Position Min | Position Max | This value changes based on user selected position units. |
| 21 | 0 | DRV.IPEAK | This value changes based on the specific AKDs drive limits. |
| 22 | 0 | 32 | See Digital Input Mode 22 for details. |
| 23 | 0 | 2056 | See Digital Input Mode 23 for details. |
Dependency on DINx.MODE
Typically, the user can set DINx.PARAM before the corresponding DINx.MODE is set. However, if DINx.PARAM is set before DINx.MODE is set, and the value of DINx.PARAM is outside the new DINx.MODE’s range, then DINx.PARAM will be set to zero.
Example:
DIN1.MODE is set to 0 by default
DIN1.PARAM is set to 200
DIN1.MODE is changed to 2 (execute motion taks)
200 is larger than the maximum for DIN1.MODE 2, so DIN1.PARAM will be set to 0 to prevent errors.
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
-9,223,372,036,854,775,000 to +9,223,372,036,854,775,000 Note: Varies based on DINx.MODE. See below. |
|
Default Value |
0 |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | No |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
| Fieldbus | Index/Subindex | Object Start Version | |
|---|---|---|---|
|
EtherCAT COE and CANopen |
3474h/1, 3474/8 |
DIN1.PARAM |
M_01-00-00-000 |
| 3474h/2, 3474/9 |
DIN2.PARAM |
||
| 3474h/3, 3474/A | DIN3.PARAM | ||
| 3474h/4, 3474/B | DIN4.PARAM | ||
| 3474h/5, 3474/C | DIN5.PARAM | ||
| 3474h/6, 3474/D | DIN6.PARAM | ||
| 3474h/7, 3474/E | DIN7.PARAM | ||
| Paramter |
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|---|
| DIN1.PARAM |
Profinet |
2062 | DWord | Yes |
| sercos® III | 8 Octets | |||
| DIN2.PARAM |
Profinet |
2067 | DWord | |
| sercos® III | 8 Octets | |||
| DIN3.PARAM |
Profinet |
2072 | DWord | |
| sercos® III | 8 Octets | |||
| DIN4.PARAM |
Profinet |
2077 | DWord | |
| sercos® III | 8 Octets | |||
| DIN5.PARAM |
Profinet |
2082 | DWord | |
| sercos® III | 8 Octets | |||
| DIN6.PARAM |
Profinet |
2087 | DWord | |
| sercos® III | 8 Octets | |||
| DIN7.PARAM |
Profinet |
2092 | DWord | |
| sercos® III | 8 Octets |
| Fieldbus | Parameter | Instance | Data Size | Data Type |
|---|---|---|---|---|
| EtherNet/IP | DIN1.PARAM | 63 | 8 Byte Signed | Varies |
| DIN2.PARAM | 68 | |||
| DIN3.PARAM | 73 | |||
| DIN4.PARAM | 78 | |||
| DIN5.PARAM | 83 | |||
| DIN6.PARAM | 88 | |||
| DIN7.PARAM | 93 |
| Fieldbus | Index/Subindex | Is 64 bit? | Attributes | Signed? | Object Start Version | |
|---|---|---|---|---|---|---|
| Modbus | 124 | DIN1.PARAM | Yes | 64 bit | Yes | M_01-03-00-000 |
| 134 | DIN2.PARAM | |||||
| 144 | DIN3.PARAM | |||||
| 154 | DIN4.PARAM | |||||
| 164 | DIN5.PARAM | |||||
| 174 | DIN6.PARAM | |||||
| 184 | DIN7.PARAM | |||||
Related Topics