EIP.CMDMAP

Description

EIP.CMDMAP can be used to set the following parameters in the dynamic portion of command assembly using the syntax EIP.CMDMAP <index> <parameter id>.

ID Parameter Data Size Data Type
383 SWLS.EN 2 Byte Integer
384 SWLS.LIMIT0 4 Byte Signed (scaled using EIP.POSUNIT*) Position
386 SWLS.LIMIT1 4 Byte Signed (scaled using EIP.POSUNIT*) Position

*Position unit values are scaled from 8 bytes to 4 bytes. This results in a loss of precision.

Read EIP.CMDMAP to display the current state of the 16 mappable portions of command assembly. A 0 represents an unassigned value.

-->EIP.CMDMAP
[0] 383
[1] 384
[2] 386
[3] 0
[4] 0
[5] 0
[6] 0
[7] 0
[8] 0
[9] 0
[10] 0
[11] 0
[12] 0
[13] 0
[14] 0
[15] 0
-->

Example

The following example maps the parameter to SWLS.EN to the dynamic portion of command assembly using its index ID.

--> EIP.CMDMAP 0 383

General Information

Type

R/W

Units

N/A

Range

See ID table below.

Default Value

0

Data Type

Integer

Start Version

M_01-13-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP Yes
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C No

Related Topics

EtherNet/IP Ansicht "Achse"