FBUS.PLLSTATE
Description
FBUS.PLLSTATE returns the status of the phase locked loop (PLL). The PLL states are as follows:
| PLL State | Description |
|---|---|
|
PLL not activated |
This state is set using FBUS.PARAM02. Not each fieldbus or operation mode needs synchronization. |
|
PLL activated, but unlocked |
The PLL is activated but has not yet been locked successfully. This state is related to the fieldbus master, as well as to the fieldbus mode of operation. |
|
PLL activated and locked |
PLL is fully operational and locked |
For more information, see the AKD CANopen Manual, Phase Locked Loop.
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
FBUS.PARAM1 TO FBUS.PARAM10, Fieldbus documentation |
|
Start Version |
M_01-02-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | No |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.