FBUS.SYNCACQUIREWND
Description
Defines the time window that is used for the starting the synchronization. If the measured (FBUS.SYNCDIST) and target time (FBUS.SYNCDIST) are within this absolute window (for a certain period) the synchronization is successful and FBUS.PLLSTATE will return the locked state.
General Information
|
Type |
NV Parameter |
|
Units |
ns |
|
Range |
5 to 100,000 ns |
|
Default Value |
12,500 ns |
|
Data Type |
Integer, U32 |
|
Start Version |
M_01-14-06-001 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | No |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Index/Subindex |
Object Start Version |
|---|---|---|
|
EtherCAT COE and CANopen |
5411h/0 |
M_01-14-06-001 |
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
3014 |
DWord | No |
| sercos® III | 4 Octets |
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 1042 | 4 Byte | Integer |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? | Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
2898 |
No | 32 bit | No | M_01-14-06-001 |