GEAR.OUT

Description

This parameter is the numerator of the gear ratio for the electronic gearing mode. The gear ratio is used in order to increase/decrease the slave velocity. The slave velocity can be calculated by the following formula:

Slave velocity = Master velocity * GEAR.OUT/GEAR.IN

 

Make sure that the external master source has been set properly. Also, be certain to select a gear ratio such that the maximum electronic gearing velocity (GEAR.VMAX) will not be exceeded.

Master velocitymax * GEAR.OUT/GEAR.IN < GEAR.VMAX

General Information

Type

NV Parameter

Units

N/A

Range

-32,768 to +32,767

Default Value

1

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

50BEh /0

M_01-00-00-000

Fieldbus

Address

Attributes Signed?

Profinet

2190

Word Yes
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 191 2 Byte Signed Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed? Object Start Version

Modbus

380

No 16 bit Yes M_01-03-00-000

Related Topics

Elektronisches Getriebe