HOME.MOVE
Description
The HOME.MOVE command starts a homing procedure. The DRV.OPMODE must be set to 2 (closed position loop) and DRV.CMDSOURCE must be set to 0 (TCP/IP command).
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | No |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
2204 |
Command* | No |
| sercos® III |
*For Profinet, write a value of 0 into the PNU to execute a command.
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 205 | Command | None |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? | Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
408 |
No | Command | No | M_01-00-00-000 |
Related Topics