HOME.PERRTHRESH

Description

This parameter is used for the homing modes against a mechanical stop (HOME.MODE = 8 and 9). The absolute value of the following error (PL.ERR ) is compared with HOME.PERRTHRESH in order to detect a mechanical stop.

General Information

Type

R/W Parameter

Units

Depends on UNIT.PROTARY or UNIT.PLINEAR

Rotary: counts, rad, deg, Benutzerspezifische Einheiten, 16-bit counts

Linear: counts, mm, µm, Benutzerspezifische Einheiten, 16-bit counts

Range

N/A

Default Value

N/A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

3482h/0

M_01-00-00-000

Fieldbus

Address

Attributes Signed?

Profinet

2207

DWord Yes
sercos® III 8 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 208 8 Byte Signed Position

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed? Object Start Version

Modbus

414

Yes 64 bit Yes M_01-03-00-000

Related Topics

Homing Mode 8: Referenzieren auf mechanischen Anschlag