MOTOR.IDMAX

Description

This parameter is supported for IPM motors (MOTOR.TYPE = 6). MOTOR.IDMAX is the maximum motor winding current in the direct (non-torque producing) axis.


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.

General Information

Type

NV Parameter

Units

Arms

Range

0.2 to 1000

Default Value

0.5 * MOTOR.IPEAK

Data Type

Float

Start Version

M_01-11-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2894

DWord No
sercos® III 4 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 895 4 Byte Float

Related Topics

Motor | MOTOR.IPEAK