MOTOR.IMID

Description

The value of IL.IMID can be estimated using the motor name plate information.

The following rule should generally be used:

In which Id is the value for IL.IMID, the preset rotor flux building current, Ir is the name plate phase current, cosϕ is the name plate power factor at rated and operation, and 0.8 is an empirical factor (accounts for the angle error due to voltage drop on the leakage induction).

General Information

Type

R/W

Units

Arms

Range

0 to DRIVE.IPEAK

Default Value

0

Data Type

Float

Start Version

M_01-08-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

5362h /0

M_01-08-00-000

Fieldbus

Address

Attributes Signed?

Profinet

2866

DWord No
sercos® III 4 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 867 4 Byte Float

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

1732

No 32-bit No

Related Topics

Motor