MOTOR.INFO

Description

MOTOR.INFO returns the production year and week of a Kollmorgen motor. This is supported under following conditions:

  • A Kollmorgen motor is used
  • The feedback has a manufacture specific memory
  • The electronic data sheet of the motor is properly programmed
  • The parameter MOTOR.AUTOSET is turned on

If one of the conditions is not true, the parameter returns:

-->MOTOR.INFO

Year: N/A

Week: N/A

If the motor was manufactured in the 36th week in 2015, the parameter returns:

-->MOTOR.INFO

Year: 2015

Week: 36

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-14-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Related Topics

Motor