MOTOR.KT
Description
This parameter is the torque constant of the motor in Nm/A.The value can be online checked according to the following equation:
Kt = 60 *√3 * Ui/( 2 * π* n)
Where:
Ui = induced voltage of the motor
n = actual rotor velocity
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET=1.
General Information
|
Type |
NV Parameter |
|
Units |
Nm/A |
|
Range |
0.001 Nm/A to 1,000,000.000 Nm/A for rotary motors. 0.001 Nm/A to 1,000,000.000 N/A for linear motors. |
|
Default Value |
0.1 Nm/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Index/Subindex |
Object Start Version |
|---|---|---|
|
EtherCAT COE and CANopen |
3593h/0 |
M_01-00-00-000 |
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
2248 |
DWord | No |
| sercos® III | 4 Octets |
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 249 | 4 Byte | Float |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
496 |
No | 32 bit | No |
M_01-03-00-000 |
Related Topics