MOTOR.PHASE
Description
This parameter sets the motor phase.
(missing or bad snippet)- When loading a parameter file to a new device, if MOTOR.AUTOSET = 0 then motor parameters should be checked to make sure they are properly configured for the motor on the new device.
General Information
Type | NV Parameter |
Units | Electrical degrees |
Range | 0 to 360° |
Default Value | 0° |
Data Type | Integer |
See Also | N/A |
Start Version | M_01-00-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus | Index/Subindex | Object Start Version |
|---|---|---|
EtherCAT COE and CANopen | 359Ch/0 | M_01-00-00-000 |
Fieldbus | Address | Attributes | Signed? |
|---|---|---|---|
Profinet | 2250 | Word | No |
| sercos® III | 2 Octets |
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 251 | 2 Byte | Integer |
Fieldbus | Index/Subindex | Is 64 bit? | Attributes | Signed? | Object Start Version |
|---|---|---|---|---|---|
Modbus | 500 | No | 16 bit | No | M_01-03-00-000 |
Related Topics