MOTOR.SERIALNUM
Description
This parameter is used to read the motor serial number.
The serial number is set during production of the motor and cannot be changed by the user.
-
- If MOTOR.AUTOSET=1 and FB1.MEMVER >= 0.05, this parameter is automatically configured for Kollmorgen motors.
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
14 chars |
|
Default Value |
N/A |
|
Data Type |
String |
|
See Also |
N/A |
|
Start Version |
M_01-18-07-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Related Topics