MOTOR.TBRAKEAPP

Description

This parameter is used to configure the mechanical delay required for the motor brake to close. When disabling the drive with DRV.DISMODE not '0 - Disable axis immediately', the drive will servo to hold position for the time set, allowing the brake to apply.

(missing or bad snippet)

General Information

Type

NV Parameter

Units

ms

Range

0 to 1,000 ms

Default Value

75 ms

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Variants Supported

VariantSupported
AKD BaseYes
AKD with Position IndexerYes
AKD EtherCATYes
AKD CANopenYes
AKD BASICYes
AKD SynqNetYes*
AKD EtherNet/IPYes
AKD ProfinetYes
AKD sercos® IIIYes
AKD-NYes
AKD-CNo

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

366Eh/0

M_01-00-00-000

Fieldbus

Address

AttributesSigned?

Profinet

2255

WordNo
sercos® III2 Octets
FieldbusInstanceData SizeData Type
EtherNet/IP2562 ByteInteger

Fieldbus

Index/Subindex

Is 64 bit?AttributesSigned?

Object Start Version

Modbus

510

No16 bitNo

M_01-03-00-000

Related Topics

Motor