REC.TRIG
Description
REC.TRIG starts the trigger according to the trigger type defined by REC.TRIGTYPE.
REC.TRIG sets the value of REC.DONE to 0.
After calling REC.TRIG, the data that was recorded by previous recording is deleted and cannot be retrieved.
No REC parameters can be set after a call to REC.TRIG until the recorder has finished or until REC.OFF is executed.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
REC.RETRIEVE, REC.OFF |
|
Start Version |
M_01-00-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
2360 |
Command* | No |
| sercos® III |
*For Profinet, write a value of 0 into the PNU to execute a command.
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 361 | Command | None |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
720 |
No | Command | No |
M_01-03-00-000 |
Related Topics