VBUS.UVFTHRESH

Description

VBUS.UVFTHRESH sets the undervoltage fault level of the DC bus.

The default value is read from the EEPROM, but can by modified by the user and stored on the NV RAM. This value varies according to drive type.

General Information

Type

R/W Parameter

Units

VDC

Range

90 to 420 VDC

Default Value

90 VDC

Data Type

Integer

See Also

VBUS.OVFTHRESH

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

361Dh/0

M_01-00-00-000

Fieldbus

Address

Attributes Signed?

Profinet

2400

Word No
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 401 2 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

800

No 16 bit No

M_01-03-00-000

Related Topics

Regeneration