VL.ARTYPE1 TO VL.ARTYPE4

Description

These parameters indicate the method used to calculate the biquad coefficients VL.ARPFx, VL.ARPQx, VL.ARZFx, and VL.ARZQx. A value of 0 indicates that the coefficients are set directly. This parameter has no effect on the filter itself, but is only used to determine the original design parameters. Currently, only the value of 0 is supported.

General Information

Type

NV Parameter

Units

N/A

Range

0

Default Value

0

Data Type

U8

See Also

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

3405h/1

VL.ARTYPE1

M_01-02-00-000

3405h/2

VL.ARTYPE2

3405h/3

VL.ARTYPE3

3405h/4

VL.ARTYPE4

Parameter

Fieldbus

Address

Attributes Signed?
VL.ARTYPE1 Profinet

2412

Byte No
sercos® III 2 Octets
VL.ARTYPE2 Profinet 2413 Byte
sercos® III 2 Octets
VL.ARTYPE3 Profinet 2414 Byte
sercos® III 2 Octets
VL.ARTYPE4 Profinet 2415 Byte
sercos® III 2 Octets

Fieldbus

Parameter

Instance

Data Size Data Type

EtherNet/IP

VL.ARTYPE1

413

1 Byte Integer

VL.ARTYPE2

414

VL.ARTYPE3

415

VL.ARTYPE4

416

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

824

VL.ARTYPE1

No 8 bit No

M_01-03-00-000

826

VL.ARTYPE2

828

VL.ARTYPE3

830

VL.ARTYPE4

Related Topics

Geschwindigkeitsregelkreis