AXIS#.SAFEPARAM.SLS_#.TIMEFORVELINLIMITS

Description

Indicates the time for the velocity in limits for the Safely Limited Speed (SLS) safety function. After this time, the monitoring can be activated if the velocity is already in the limits. This is the time the velocity has to be within the limits before the final state is activated.

 

This value is t_L_SLS in the following diagram:

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 60000]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.TIMEFORVELINLIMITS

315ch

06h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.TIMEFORVELINLIMITS

315dh

06h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.TIMEFORVELINLIMITS

315eh

06h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.TIMEFORVELINLIMITS

325ch

06h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.TIMEFORVELINLIMITS

325dh

06h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.TIMEFORVELINLIMITS

325eh

06h

Unsigned16

-

-

Read/Write

No