AXIS#.SAFE.SOS_x.ACTIVE
Description
Indicates whether the Safe Operating Stop (SOS) function instance is active.
Value |
Description |
---|---|
0 |
Not active |
1 |
Active |
Context
For complete SOS information refer to SOS (Safe Operating Stop).
Related safety parameters:
- AXIS#.SAFE.SOS_x.INTERNALSTATE
- AXIS#.SAFEPARAM.SOS_x.FSOE
- AXIS#.SAFEPARAM.SOS_x.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SOS_x.POSZEROWINDOW
- AXIS#.SAFEPARAM.SOS_x.RESTARTACKBEHAVIOR
- AXIS#.SAFEPARAM.SOS_x.SAFEINPUT
- AXIS#.SAFEPARAM.SOS_x.TIMEDELAYMONITORING
- AXIS#.SAFEPARAM.SOS_x.VELMONITOREN
- AXIS#.SAFEPARAM.SOS_x.VELZEROWINDOW
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0, 1 |
Default Value |
N/A |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SAFE.SOS_2.ACTIVE |
666fh |
02h |
Unsigned8 |
- |
- |
Read only |
Yes |
AXIS2.SAFE.SOS_2.ACTIVE |
6e6fh |
02h |
Unsigned8 |
- |
- |
Read only |
Yes |