AXISx.MOTIONSTAT.SETTLED

Description

This parameter indicates whether the axis has settled. An axis is considered settled when both its settling position window (AXIS#.SETTLE.P) and settling velocity window (AXIS#.SETTLE.V) constraints are met for the duration specified by AXIS#.SETTLE.T.

This value is also indicated in the AXIS#.MOTIONSTAT word, as Bit 26.

Versions

Action Version Notes
Implemented 02-13-01-000 --

General Information

Type

Read Only

Units

N/A

Range

0 - 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5039

1

5039 (0x13af)

AXIS1.MOTIONSTAT.SETTLED

Unsigned8

Read Only

Yes

70575

2

5039 (0x13af)

AXIS2.MOTIONSTAT.SETTLED

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTIONSTAT.SETTLED

5039

Unsigned8

Read Only

-

Related Topics

AXIS#.MOTIONSTAT

AXIS#.SETTLE.T