AXIS#.SETTLE.T

Description

Within AXIS#.MOTIONSTAT, AXIS#.SETTLE.T is used as the time in milliseconds during which both the target velocity of a move and its target position have to be within the windows specified respectively by AXIS#.SETTLE.V and AXIS#.SETTLE.P for the motion to be considered settled. AXIS#.MOTIONSTAT displays a "Settled" bit to indicate when this condition is reached.

Versions

Action Version Notes
Implemented 02-13-01-000 -

General Information

Type

Read Write

Units

ms

Range

0 - 65535

Default Value

100 ms

Data Type

Unsigned Integer

See Also

AXIS#.MOTIONSTAT, AXISx.MOTIONSTAT.SETTLED

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SETTLE.T

5016h

03h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7102

1

7102 (0x1bbe)

AXIS1.SETTLE.T

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.SETTLE.T

7102

Unsigned16

Read/Write

-