AXIS#.PL.CMD.OFFSET

Description

This parameter displays the sum of all position loop offset signals (See AXIS#.PL.CMD.FBUSOFFSET, AXIS#.PL.CMD.MWOFFSET).

These values will be added to any active trajectory values from the drive trajectory generator, external electronic gearing command, analog command and fieldbus command.

Versions

Action Version Notes
Implemented 02-08-02-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.CMD.OFFSET

500ch

17h

Signed32

Position

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5920

1

5920 (0x1720)

AXIS1.PL.CMD.OFFSET

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.PL.CMD.OFFSET

5920

Signed32

Read Only

Position