AXIS#.UNIT.VROTARY
Description
AXIS#.UNIT.VROTARY sets the velocity units when the motor type (AXIS#.MOTOR.TYPE) is rotary.
|
Value |
Units |
|---|---|
|
0 |
RPM |
|
1 |
RPS |
|
2 |
deg/s |
|
3 |
Custom Units/s |
| 4 | rad/s |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 4 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.UNIT.VROTARY |
5010h |
04h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6607 |
1 |
6607 (0x19cf) |
AXIS1.UNIT.VROTARY |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.UNIT.VROTARY |
6607 |
Unsigned8 |
Read/Write |
- |