AXIS#.VL.CMDU

Description

AXIS#.VL.CMDU sets the user velocity command. When AXIS#.OPMODE is set to 1 (velocity loop) and AXIS#.CMDSOURCE is set to 0 (TCP/IP channel), then setting this value when the drive is enabled will cause the drive to rotate at the required velocity.

This velocity command will be a step command to the service motion velocity.

When in use, the Service Motion Status bit will indicate motion is active.

The acceleration and deceleration slopes to reach the desired velocity are shared with the Service Motion keywords SM.ACC and SM.DEC.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read/Write

Units

Depends on AXIS#.UNIT.VROTARY

Rotary: rpm, rps, deg/s, custom units/s, rad/s

Range

Rotary

-15,000.000 to 15,000.000 rpm

-250.000 to 250.000 rps

-90000.000 to 90000.000 deg/s

-1250.000 to 1250.000 custom units/s

-1570.796 to 1570.796 rad/s

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6022

1

6022 (0x1786)

AXIS1.VL.CMDU

Signed32

Read/Write

Yes

71558

2

6022 (0x1786)

AXIS2.VL.CMDU

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.CMDU

6022

Float

Read/Write

Velocity

Related Topics

"Velocity Loop"