Motor Cable Connection
Motors with two wire feedback systems like SFD-M can be connected to the servo drive by using a single Kollmorgen hybrid cable.
Motor power and brake connector X1
|
|
|
Motor leads to servo drive connector X1
|
Pin |
Signal |
Description |
|---|---|---|
| 1 | BRAKE- | Negative connection to the mechanical brake |
| 2 | BRAKE+ | Positive connection to the mechanical brake |
| 3 | PE | Protective earth |
| 4 | U | Connection to motor phase |
| 5 | V | Connection to motor phase |
| 6 | W | Connection to motor phase |
|
Pin |
Signal |
Description |
|---|---|---|
| 1 | BRAKE- | Negative connection to the mechanical brake |
| 2 | BRAKE+ | Positive connection to the mechanical brake |
| 3 | PE | Protective earth |
| 4 | ||
| 5 | U | Connection to motor phase |
| 6 | V | Connection to motor phase |
| 7 | W | Connection to motor phase |
Motor feedback cable connector to servo drive feedback connector X23
|
Pin |
Signal |
Description |
|---|---|---|
| 1 | COM+ | SFD-M Positive Signal |
| 2 | COM- | SFD-M Negative Signal |