MLMotionRstErr
Function - Clears motion engine errors, motion bus driver errors, and EtherCAT network errors.
- Re-initializes the motion engine after a motion error.
- MLMotionRstErr returns the motion engine status to the Stopped state if an error condition was cleared successfully.
- Motion errors are for example communication errors of the motion bus.
- Returns TRUE if the function succeeded.
Inputs
There are no Inputs for this function / function block.
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE if errors have been reset. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Reset and restart motion engine
//Done to restart EtherCAT after controller error such as
//E30 or E33 that stops network communication
//First have to reset error, then start network again
ON ResetMotionEngineError DO
MLMotionRstErr();
END_DO;
MotionEngineStatus:= MLMotionStatus();
ON StartMotionEngine DO
MLMotionStart();
END_DO;
See Also