MC_MoveContVel

PLCopen motion icon

 Function Block - Performs a single-axis non-ending move at a specified velocity with the option of continually updating the ongoing motion with the current input parameters.


    • This function block starts a motion-related action and stores data for calculations and error checking.
    • If using a dual-core controller, see Program a Multi-Core Controller.
  • After MC_MoveContVel execution begins (Execute input - low to high), follow up changes to input parameters immediately affect the ongoing motion, without requiring an additional low to high transition on the Execute input.
  • This type of move can be terminated with the MC_Halt function block or by aborting it with another move.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, request to queue the move.

Axis

AXIS_REF

1 to 256

N/A

No default

Name of a declared instance of the AXIS_REF library function.

Velocity

LREAL

All finite values.

User units / sec

No default

The target axis velocity.

  • Negative values of velocity move the axis in the negative direction.
  • Positive values move the axis in the positive direction.
  • A value of 0 (zero) is valid.
    • 0 (zero) indicates a deceleration to zero velocity.

Acceleration

LREAL

Positive values.

User units / sec2

No default

Deceleration

LREAL

Positive values.

User units / sec2

No default

Jerk

LREAL

No range

User units / sec3

No default

ContinuousUpdate

BOOL

FALSE, TRUE

N/A

No default

Determines if the inputs of the function block are re-evaluated every cycle or if they are only evaluated on the rising edge of Execute.

  • If TRUE, when the function block is triggered (on the rising edge of Execute), the function block uses the current updated values of the input variables and apply it to the ongoing movement of the axis.
    • This continues as long as ContinuousUpdate stays TRUE.
  • The impact of ContinuousUpdate ends as soon as the function block is no longer busy (Busy output is FALSE) or ContinuousUpdate is set to FALSE.

BufferMode

SINT

Enumerated

N/A

No default

The specified buffer mode.

  • BM_ABORTING
  • BM_BUFFERED
  • BM_BLENDING_PREVIOUS
  • BM_BLENDING_NEXT
  • BM_BLENDING_LOW
  • BM_BLENDING_HIGH
  • See Buffer Modes.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

InVelocity

BOOL

FALSE, TRUE

N/A

Indicates the command velocity has reached the programmed velocity.

Busy

BOOL

FALSE, TRUE

N/A

High from the moment the Execute input goes high until the time the move is ended.

Active

BOOL

FALSE, TRUE

N/A

Indicates this move is the Active move.

CommandAborted

BOOL

FALSE, TRUE

N/A

If TRUE, the command was aborted by another function block.

Error

BOOL

FALSE, TRUE

N/A

Indicates either:

  • An invalid input was specified.
  • The move was terminated due to an error.

ErrorID

INT

-32768 to +32767

N/A

Time Diagram

This example shows the behavior of the combination of a MC_Stop function block with a MC_MoveContVel function block.

  • A rotating axis is ramped down with FB2 MC_Stop.
  • The axis rejects motion commands as long as MC_Stop parameter Execute = TRUE.
  • FB1 MC_MoveContVel reports an error indicating the busy MC_Stop command.

Figure 1: Time Diagrams: First and Second FBs

Figure 2: Time Diagram

FBD Language Example

Not available.

FFLD Language Example

IL Language Example

Not available.

ST Language Example

(* MC_MoveContVel ST example *)
Inst_MC_MoveContVel( MovVelReq , Axis1, Vel, 100.0, 100.0, 0, True, MC_BUFFER_MODE_ABORTING );

See Also