MC_MoveRelative

PLCopen motion icon

 Function Block - Performs a single-axis move of a specified distance relative to the actual position at the time of the start of execution.


    • This function block starts a motion-related action and stores data for calculations and error checking.
    • If using a dual-core controller, see Program a Multi-Core Controller.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, request to queue the move.

Axis

AXIS_REF

1 to 256

N/A

No default

Name of a declared instance of the AXIS_REF library function.

Distance

LREAL

No range

User units

No default

Distance.

Velocity

LREAL

No range

User units / sec

No default

Velocity setpoint.

Acceleration

LREAL

No range

User units / sec2

No default

Deceleration

LREAL

No range

User units / sec2

No default

Jerk

LREAL

No range

User units / sec3

No default

BufferMode

SINT

Enumerated

N/A

No default

The specified buffer mode.

  • BM_ABORTING
  • BM_BUFFERED
  • BM_BLENDING_PREVIOUS
  • BM_BLENDING_NEXT
  • BM_BLENDING_LOW
  • BM_BLENDING_HIGH
  • See Buffer Modes.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

Indicates the move completed successfully.
The Command Position has reached the endpoint.

Busy

BOOL

FALSE, TRUE

N/A

High from the moment the Execute input goes high until the time the move is ended.

Active

BOOL

FALSE, TRUE

N/A

Indicates this move is the Active move.

CommandAborted

BOOL

FALSE, TRUE

N/A

If TRUE, the command was aborted by another function block.

Error

BOOL

FALSE, TRUE

N/A

Indicates either:

  • An invalid input was specified.
  • The move was terminated due to an error.

ErrorID

INT

No range

N/A

Time Diagram

These images show two examples of the combination of two relative move Function Blocks (FBs).

  • The left part of the diagram illustrates when the second FB is called after the first one.
    • If the first reaches the commanded position of 6000, and the velocity is 0 (zero), the output Done causes the second FB to move to the distance 10000.
  • The right part of the diagram illustrates when the second move FB starts the execution while the first FB is still executing. 
    • The first motion is interrupted and aborted by the Test signal during the constant velocity of the first FB.
    • The second FB adds on the actual position of 3250 the distance 4000 and moves the axis to the resulting position of 7250.

Figure 1: Time Diagrams: First and Second FBs

Figure 2: Time Diagram

FBD Language Example

Not available.

FFLD Language Example

IL Language Example

Not available.

ST Language Example

(* MC_MoveRelative ST example *)
Inst_MC_MoveRelative( MovRelReq, Axis1, 10.0, 200.0,150.0, 150.0, 0,0 );
MovRelDone := Inst_MC_MoveRelative.Done; //store Done output into user defined variable

See Also