MLAxisGenReadAcc

Pipe Network motion icon

 Function - Gets the acceleration of the internal generator of an axis.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Acceleration

LREAL

No range

User units / sec2

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Acceleration := MLAxisGenReadAcc( PipeNetwork.Axis1 );

See Also