MLAxisGenReadSpd

Pipe Network motion icon

 Function - Gets the speed of the internal generator of an axis.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Speed

LREAL

No range

User units / sec

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Speed := MLAxisGenReadSpd( PipeNetwork.Axis1 ) ;

See Also