MLAxisRstFastIn

Pipe Network motion icon

 Function - Writes in the Latch Control Word to reset the Fast Input.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

InputID

DINT

See Description.

N/A

No default

ID name of the Fast input of an axis (i.e., IN1 and IN2 on S300).

Valid values of InputID are:

  • 0 = Touch Probe 1 / Capture Engine 0
  • 1 = Touch Probe 2 / Capture Engine 1

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 MLAxisRstFastIn(PipeNetwork.Axis1, 0 )  ;

See Also